Something We All Do
In this episode of CADDY TV Rick discusses how to attach the pipe to strut with three different styles of pipe clamp including:
RIGD/COPC are one piece strut clamps. Both of them install the same way but are made of different materials for use with different types of pipe. The RIGD is for use with rigid pipe or conduit, and the COPC is specifically designed for use with copper pipe. Installation is very easy; the installer simply needs to break the piece in two and attach the two parts with the pre-threaded bolt. A plastic washer on the bolt ensures that the hardware will not be lost or dropped.
TSM/TSMI are one piece plastic strut clips that snap into the strut and then are twisted to secure them in place. Pipe or conduit easily snaps in, and the plastic finish allows it to be used with copper.